SLAU847E October 2022 – May 2025 MSPM0L1105 , MSPM0L1106 , MSPM0L1116 , MSPM0L1117 , MSPM0L1227 , MSPM0L1227-Q1 , MSPM0L1228 , MSPM0L1228-Q1 , MSPM0L1303 , MSPM0L1304 , MSPM0L1304-Q1 , MSPM0L1305 , MSPM0L1305-Q1 , MSPM0L1306 , MSPM0L1306-Q1 , MSPM0L1343 , MSPM0L1344 , MSPM0L1345 , MSPM0L1346 , MSPM0L2227 , MSPM0L2227-Q1 , MSPM0L2228 , MSPM0L2228-Q1
DMA_TRIG1 and DMA_TRIG0 registers are used to setup the trigger signaling for the DMA. This can be setup in a flexible way to trigger the DMA for Controller or Target and receive or transmit events with the following four trigger conditions:
| IIDX STAT | Name | Description |
|---|---|---|
| 0x01 | MRXFIFOTRG | Controller receive FIFO trigger. Trigger when RX FIFO contains >= defined bytes |
| 0x02 | MTXFIFOTRG | Controller transmit FIFO trigger. Trigger when Transmit FIFO contains <= defined bytes |
| 0x03 | SRXFIFOTRG | Target receive FIFO trigger. Trigger when RX FIFO contains >= defined bytes |
| 0x04 | STXFIFOTRG | Target transmit FIFO trigger. Trigger when Transmit FIFO contains <= defined bytes |
The DMA trigger event configuration is managed with the DMA_TRIG1 and DMA_TRIG0 event management registers. See Section 7.2.5 for guidance on configuring the Event registers and Section 7.1.3.2 for on how DMA trigger event works. DMA_TRIG1 and DMA_TRIG0 are two event management registers that correspond to two DMA channels.
As shown in Figure 22-17, each DMA channel can be triggered by any of the conditions listed in Table 22-76 and it can generate either the controller DMA done signal or target DMA done signal.
For example, the user can configure the DMA_TRIG1 trigger using MTXFIFOTRG and the DMA_TRIG0 trigger using SRXFIFOTRG. When the Channel 1 DMA status changes to done, the MDMA_DONE_TX and MDMA_DONE_RX interrupts will set, and when the Channel 2 DMA status change to done, the SDMA_DONE_TX and SDMA_DONE_RX interrupts will set.