SLAU847E October 2022 – May 2025 MSPM0L1105 , MSPM0L1106 , MSPM0L1116 , MSPM0L1117 , MSPM0L1227 , MSPM0L1227-Q1 , MSPM0L1228 , MSPM0L1228-Q1 , MSPM0L1303 , MSPM0L1304 , MSPM0L1304-Q1 , MSPM0L1305 , MSPM0L1305-Q1 , MSPM0L1306 , MSPM0L1306-Q1 , MSPM0L1343 , MSPM0L1344 , MSPM0L1345 , MSPM0L1346 , MSPM0L2227 , MSPM0L2227-Q1 , MSPM0L2228 , MSPM0L2228-Q1
The CRC generator is initialized by configuring the desired mode of operation in the CRCCTRL register, followed by writing the seed value to the CRCSEED register. After the seed is loaded to the CRCSEED register, the CRCOUT register will reflect the SEED value loaded to CRCSEED.
Once initialized, data can be input into the CRC generator by writing to the CRCIN register using byte (8-bit), half-word (16-bit), or word (32-bit) writes. The CPU or the DMA can be used to move input data into the CRC accelerator.
When using the CRC generator to verify a data set, all data to be included in the CRC calculation must be written to the CRCIN register in the same order as was used to calculate the original CRC signature. When using the CRC generator to create a new signature to be used in the future for verification, be sure to load the data the same way and with the same settings when performing verification.
The current CRC output can be read at any time by reading the CRCOUT register.