SLAU858B December 2023 – June 2025 AFE881H1
To launch the software, locate the Texas Instruments folder in the All Programs menu, and select the AFE88xH1EVM icon.
Once the software has launched, a pop-up window prompts the user to select what EVM is being used. If using the AFE881H1EVM, then select the AFE881H1EVM option.
Next, shown in Figure 3-5, the user can select between the 3 different communication modes the AFE881H1 supports. Specific requirements and functionality for the different modes are detailed in the AFEx81H1 16-Bit and 14-Bit, Low-Power DACs With Internal HART® Modem, Voltage Reference, and Diagnostic ADC for 4mA to 20mA Loop-Powered Applications data sheet.
When the user selects a mode, the SDO, CONFIG, and UBM registers are updated to support immediate communication. The default values of all other registers are reflected in the GUI.
Figure 3-6 shows that if the onboard FTDI controller is connected correctly, the status bar at the bottom of the screen displays CONNECTED. If the controller is not properly connected or not connected at all, the status displays DEMO. If the graphical user interface (GUI) is not displaying the CONNECTED status while the EVM is connected, then unplug and reconnect the EVM, and then relaunch the GUI software.
Figure 3-6 AFE88xH1EVM GUI Connection
Detection