SLAU957 June   2025 TRF1108 , TRF1208

 

  1.   1
  2.   Description
  3.   Get Started
  4.   Features
  5.   Applications
  6.   6
  7. 1Evaluation Module Overview
    1. 1.1 Introduction
    2. 1.2 Kit Contents
    3. 1.3 Specification
    4. 1.4 Device Information
  8. 2Hardware
    1. 2.1 Power Requirements
    2. 2.2 Setup
    3. 2.3 Interfaces
  9. 3Software
    1. 3.1 Software Installation
    2. 3.2 Software Description
      1. 3.2.1 HSDC Pro Overview
      2. 3.2.2 Latte Overview
        1. 3.2.2.1 Latte Shortcuts
  10. 4Implementation Results
    1. 4.1 Evaluation Setup TRF-LSC-AFE7950EVM Automatic Configuration
      1. 4.1.1 Recommended Test Environment
      2. 4.1.2 Required Hardware
      3. 4.1.3 Steps to Start Automatic Configuration
      4. 4.1.4 TXDAC Evaluation
      5. 4.1.5 RXADC and FBADC Evaluation
      6. 4.1.6 TRF-LSC-AFE7950EVM Manual Configuration
        1. 4.1.6.1 TSW14J5x DAC Pattern Setup
        2. 4.1.6.2 Connect Latte to Board
        3. 4.1.6.3 Compile Libraries
        4. 4.1.6.4 Program TRF-LSC-AFE7950EVM
        5. 4.1.6.5 Modify Configuration
      7. 4.1.7 Setup the TSW14J5x With the HSDC PRO
        1. 4.1.7.1 DAC Pattern Setup and Send
        2. 4.1.7.2 DAC Synchronization Check
        3. 4.1.7.3 ADC Data Capture
        4. 4.1.7.4 ADC Synchronization Check
    2. 4.2 Status Check and Troubleshooting Guidelines
      1. 4.2.1 EVM Status Indicators
      2. 4.2.2 TSW14J56 EVM
    3. 4.3 Performance Data and Results
  11. 5Hardware Design Files
    1. 5.1 Schematics
    2. 5.2 PCB Layouts
    3. 5.3 Bill of Materials (BOM)
  12. 6Additional Information
    1. 6.1 Trademarks

DAC Pattern Setup and Send

This section lists the steps to create and send a DAC pattern from the TSW14J5x board.

  1. Click on the HSDC PRO DAC tab. Figure 4-10 shows a brief description of the DAC tab.
    TRF-LSC-AFE7950EVM HSDC PRO DAC Tab
                            Overview Figure 4-10 HSDC PRO DAC Tab Overview
  2. Figure 4-11 shows a pictorial representation to create and send a sinusoid.
    TRF-LSC-AFE7950EVM Setup a
                            Sinusoid Figure 4-11 Setup a Sinusoid
  3. How to create and send a sinusoid is outlined in the following steps:
    1. Select AFE79xx_2x2TX_44210 in the device-specific initialization option. Click Yes if prompted to download the firmware (FW). The default option is to run the board in the transceiver mode of operation, which enables simultaneous operation of the TX and the RX and FBRX. The FW used in transceiver mode has the letters XCVR in the name.
    2. Enter 491.52 M as the data rate and 0.9 for a scaling factor.
    3. Create a sinusoid by entering the frequency in the Tone Generator section of the HSDC PRO window.
    4. Press Send to transmit the DAC pattern to the TRF-LSC-AFE7950EVM. Figure 4-12 shows the resulting message with the lane rate and reference clock expected in the FPGA. Click OK.
TRF-LSC-AFE7950EVM HSDC PRO Lane and Reference
                    Clock Rate Pop-Up Figure 4-12 HSDC PRO Lane and Reference Clock Rate Pop-Up

Figure 4-13 shows an example setup with a 100MHz sinusoid.

TRF-LSC-AFE7950EVM HSDC PRO CW Figure 4-13 HSDC PRO CW

Alternatively, load a pattern file (for example, LTE) and send using the Load External Pattern File button.

The DAC setup is now complete.