Follow the steps below when connecting an
MSPM0 LaunchPad to a DRV83xx EVM:
- Connect the three motor phase terminals
to the driver board (phases A, B, and C). If the motor has a center tap connection or
wires for Hall-effect sensors, leave these wires unconnected.
- Make the inter-device connections from
the MSPM0 LaunchPad kit to the DRV83xx EVM by mating the EVM to the LaunchPad kit or using
jumper wires as shown in Figure 2-4. For hardware user guide connection details, see Section 2.1.1.
Note: If using
the GUI to communicate to the MSPM0 device using USB to backchannel UART, connect the
backchannel UART connections to UART3_TX and UART3_RX as shown in
Figure 2-5/
Figure 2-6
- Connect a micro-USB cable from the MSPM0
LaunchPad kit to the PC.
- Remove GND and 3V3 isolation jumpers
on the bridge if desired to isolate the PC from the motor system. If this step is
done, 3V3 must be provided externally or from the DRV83xx EVM board, if
available.
- Supply a voltage compliant with the Power
Supply Voltage (VM) range. For the recommended voltage range, see the board-specific
user's guide or DRV-specific data sheet.
-
Note: If a different UARTn port is used to
connect the serial pins, configure appropriate UART instance pins in the SYSCONFIG file of
the CCS project.