SLAZ709A October 2017 – June 2025 MSP432E401Y , MSP432E411Y
Counter does not immediately reset to 0 when MATCH is reached in edge count up mode
When configured for input edge count mode and count up mode, after counting to the match value, the counter uses one additional edge to reset the timer to 0. As a result, after the first match event, all subsequent match events occur after the programmed number of edge events plus one.
In software, account for one additional edge in the programmed edge count after the first match interrupt is received.