SLLA486A May 2020 – May 2021 ISO1042 , ISO1042-Q1 , ISO1044 , ISO1050 , ISOW1044
The CAN packet (shown in Figure 14-2) is made up of ID bits at the start of packet which are used for bitwise arbitration to determine the priority over which node will continue transmission and which other node(s) will stop. Also, towards the end of packet, ACK is acknowledgment bit which is driven dominant by all nodes which correctly receive the packet. So when multiple nodes on bus drive dominant at the same time, the differential voltage is higher in amplitude as opposed to other bits which are just driven by master transmitter node. Figure 14-3 shows a snapshot of CAN bus traffic with three nodes communicating, where we can clearly see larger voltage magnitude on CAN bus. These time instances are during acknowledgment bit or when B and C are transmitting together during ID phase.