SLLU336A May 2021 – January 2022 MCT8316A
The GUI should automatically connect to the EVM, as shown on the status bar located on the bottom of this GUI.
If the GUI doesn't connect automatically, please ensure that the "FTDI" serial port is selected by going to the top menu "Options -> Serial Port ...". Then click on the chain link icon on the left of the status bar to connect to the EVM.