SLUSDN6D September 2019 – June 2026 TPSM82810 , TPSM82813
PRODMIX
This pin sets two different parameters independently:
A resistor from COMP/FSET to GND changes the compensation as well as the switching frequency. The change in compensation adapts the device to different values of output capacitance. The resistor must be placed close to the pin to keep the parasitic capacitance on the pin to a minimum. The compensation setting is set after enabling the converter, so a change in the resistor during operation only has an effect on the switching frequency but not on the compensation.
To save external components, the pin can also be directly tied to VIN or GND to set a pre-defined switching frequency and compensation. Do not leave the pin floating.
The switching frequency must be selected based on the maximum input voltage and the output voltage to meet the specifications for the minimum on-time.
Example: VIN = 5.5V, VOUT = 1V
The compensation range has to be chosen based on the minimum effective capacitance used. The capacitance can be increased from the minimum value as given in Table 8-1 up to the maximum of 470µF in all of the three compensation ranges. The higher compensation settings give better load transient response, when larger output capacitances are used. If the capacitance of an output changes during operation, for example, when load switches are used to connect or disconnect parts of the circuitry, the compensation has to be chosen for the minimum capacitance on the output. Compensating for large output capacitance but placing less capacitance on the output can lead to instability.
The value of RCF for the intended switching frequency and compensation setting is determined by the equations in the following table.
| COMPENSATION | RCF | SWITCHING FREQUENCY | MINIMUM OUTPUT CAPACITANCE FOR VOUT < 1V | MINIMUM OUTPUT CAPACITANCE FOR 1V ≤ VOUT < 3.3V | MINIMUM OUTPUT CAPACITANCE FOR VOUT ≥ 3.3V |
|---|---|---|---|---|---|
| for smallest output capacitance (comp setting 1) |
1.8MHz (10kΩ) ... 4MHz (4.5kΩ) | 53µF | 32µF | 27µF | |
| for medium output capacitance (comp setting 2) |
1.8MHz (33kΩ) ... 4MHz (15kΩ) | 100µF | 60µF | 50µF | |
| for large output capacitance (comp setting 3) |
1.8MHz (100kΩ) ... 4MHz (45kΩ) | 200µF | 120µF | 100µF | |
| for smallest output capacitance (comp setting 1) |
tied to GND | internally fixed 2.25MHz | 53µF | 32µF | 27µF |
| for large output capacitance (comp setting 3) |
tied to VIN | internally fixed 2.25MHz | 200µF | 120µF | 100µF |
Refer to Section 9.2.2.5 for further details on the output capacitance required depending on the output voltage. All values are the effective value of capacitance.
A too high resistor value for RCF is read as "tied to VIN", and a value below the lowest range as "tied to GND". The minimum output capacitance in Table 8-1 is for capacitors close to the output of the device. If the capacitance is distributed, a lower compensation setting can be required.