SLUSG21B May 2025 – January 2026 UCC25661
PRODUCTION DATA
By implementing input voltage feed forward, the FBReplica is proportional to the input power and inversely proportional to the magnitude of the resonant tank capacitance. Rewriting the Equation 4 with input voltage feedforward applied.
Where K1 and K2 are internal synthesizer gains. The input voltage to the LLC power stage is periodically sensed on the BLK pin. A periodic average of the input voltage is used to adjust the feed forward gain to make the control signal proportional to input power. More details are found in Section 7.3.2.