SLUUAQ3A April 2016 – October 2022 BQ4050
Cell balancing in the BQ4050 device is accomplished by connecting an external parallel bypass load to each cell of the associated AFE, and enabling the bypass load depending on each cell's charge state. The bypass load is typically formed by a P-CH MOSFET and a resistor connected in series across each battery cell. The filter resistors that connect the cell tabs to VC1~VC15 pins of the associated AFE are required to be 1 kΩ.
Using this circuit, the BQ4050 balances the cells during charge by enabling the bypass around those cells above the threshold set in Cell Balance Threshold if the maximum difference in cell voltages exceeds the value programmed in Cell Balance Min. During cell balancing, the BQ4050 measures the cell voltages at an interval set in Cell Balance Interval.
The cell(s) to be balanced are prioritized by highest cell voltage but the BQ4050 will not try to balance adjacent cells. If adjacent cells need to be balanced, the BQ4050 will alternate between the highest and next-highest adjacent cells until they are balanced.
On the basis of the cell voltages, the BQ4050 either selects the appropriate cell to discharge or adjusts the cell balance threshold up by the value programmed in Cell Balance Window when all cells exceed the cell balance threshold or the highest cell exceeds the cell balance threshold by the cell balance window.
More in-depth details and data on this cell balancing algorithm can be found in: http://www.ti.com/lit/slva155.
Figure 7-1 Cell BalancingCell balancing only occurs when charging current is detected, and on non-adjacent cells at the same time. The cell balance threshold is reset to the value in Cell Balance Threshold at the start of every charge cycle. The threshold is only adjusted once during any balance interval.
The configuration data flash is stored in Advanced Charging Algorithms: Cell Balancing Config.