SLUUBH3A November 2016 – February 2022 TPS546C20A
In order to evaluate the efficiency of the power train (device and inductor), it is important to measure the voltages at the correct location. This is necessary because otherwise the measurements will include losses that are not related to the power train itself. Losses incurred by the voltage drop in the copper traces and in the input and output connectors are not related to the efficiency of the power train, which should not be included in efficiency measurements.
Input current can be measured at any point in the input wires, and output current can be measured anywhere in the output wires of the output being measured.
Table 6-2 shows the measurement points for input voltage and output voltage. VIN and VOUT are measured to calculate the efficiency. Using these measurement points will result in efficiency measurements that excluded losses due to the connectors and PCB traces.
| Test Point | Node Name | Description | Comment |
|---|---|---|---|
| VOUT | |||
| TP7 | PVIN1 | Input voltage measurement point for VIN1+ | The pair of test points are connected to the PVIN/GND pins of U1. The voltage drop between input terminal to the device pins is excluded for efficiency measurement. |
| TP23 | PGND1 | Input voltage measurement point for VIN1– (GND) | |
| TP28 | Eff_Vo1 | Output voltage measurement point for VOUT1+ | The pair of test points are connected to the closest points of Vout /GND to the inductor. The voltage drop from the output point of inductor to the output terminals is excluded for efficiency measurement. |
| TP34 | Eff_GND1 | Output voltage measurement point for VOUT1– (GND) | |