SLUUCH3 May   2021

 

  1.   Trademarks
  2. 1Introduction
    1. 1.1 Performance Specification
    2. 1.2 Modifications
  3. 2Setup
    1. 2.1 Input/Output Connector Descriptions
    2. 2.2 Setup
  4. 3TPS628690EVM-135 Test Results
  5. 4Board Layout
  6. 5Schematic and List of Materials
    1. 5.1 Schematic
    2. 5.2 List of Materials
  7. 6Software User Interface
    1. 6.1 Software Setup
    2. 6.2 Interface Hardware Setup
    3. 6.3 User Interface Operation
      1. 6.3.1 Home Screen
      2. 6.3.2 Settings Screen

Input/Output Connector Descriptions

    J1, Pin 1, 2 and 3– VINPositive input connection from the input supply for the EVM
    J1, Pin 4, 5 and 6 – GNDInput return connection from the input supply for the EVM
    J2, Pin 1 ,2 and 3– VOUTOutput voltage connection
    J2, Pin 4, 5 and 6 – GNDOutput return connection
    J3, Pin 5 – VBUS The VBUS pin of this header is used to bias the SCL and SDA nodes of I²C interface via a resistor.
    J3, Pin 6 – GNDThe GND pin of this header is used to connect the grounds of the IC and the I²C interface.
    J3, Pin 9 – SCLConnect the pin of this header to the SCL of the I²C interface.
    J3, Pin 10 – SDAConnect the pin of this header to the SDA of the I²C interface.
    JP1 – VID/PGVID/ PG pin jumper. Place the jumper across VID/ PG and LOW pins before start-up. This sets the output voltage and device address. After start-up, VOUT reflects the value set on VOUT Register 1 if the jumper is placed across VID/ PG and LOW pins. VOUT follows the value set on VOUT Register 2 if the jumper is placed across VID/ PG and HIGH pins.
    JP2 – ENEN pin input jumper. Place the jumper across ON and EN to turn on the IC. Place the jumper across OFF and EN to turn off the IC.