SLUUDB4 June 2025 TAS5830
The Automatic Gain Limiter (AGL) is a feedback mechanism that can be used to automatically control the audio signal amplitude or dynamic range within specified limits. The automatic gain limiting is done by sensing the audio signal level using an alpha filter energy structure at the output of the AGL then adjusting the gain based on whether the signal level is above or below the defined threshold. Three decisions made by the AGL are engage, disengage, or do nothing. The rate at which the AGL engages or disengages depends on the attack and release settings respectively.
Figure 3-16 shows the AGL Tuning Window. By default, the AGL is disabled and can be enabled by clicking the ON/OFF switch on the top right corner.
Figure 3-16 AGL Tuning Window
Figure 3-17 AGL Attack and Release