SLUUDC5A September   2025  – August 2026 F28E120SB , F28E120SC

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
    1. 1.1 Reference Material
    2. 1.2 Function Listing Format
  5. 2TMS320F28E12x Flash API Overview
    1. 2.1 Introduction
    2. 2.2 API Overview
    3. 2.3 Using API
      1. 2.3.1 Initialization Flow
        1. 2.3.1.1 After Device Power Up
        2. 2.3.1.2 Flash Wrapper and Bank Setup
        3. 2.3.1.3 On System Frequency Change
      2. 2.3.2 Building With the API
        1. 2.3.2.1 Ojbects Library Files
        2. 2.3.2.2 Distribution Files
        3. 2.3.2.3 Key Facts For Flash API Usage
  6. 3API Functions
    1. 3.1 Initialization Functions
      1. 3.1.1 Fapi_initializeAPI()
    2. 3.2 Flash State Machine Functions
      1. 3.2.1  Fapi_setActiveFlashBank()
      2. 3.2.2  Fapi_setupBankSectorEnable()
      3. 3.2.3  Fapi_issueAsyncCommandWithAddress()
      4. 3.2.4  Fapi_issueBankEraseCommand()
      5. 3.2.5  Fapi_issueProgrammingCommand()
      6. 3.2.6  Fapi_issueProgrammingCommandForEccAddresses()
      7. 3.2.7  Fapi_issueAutoEcc512ProgrammingCommand()
      8. 3.2.8  Fapi_issueDataAndEcc512ProgrammingCommand()
      9. 3.2.9  Fapi_issueDataOnly512ProgrammingCommand()
      10. 3.2.10 Fapi_issueEccOnly64ProgrammingCommand()
      11. 3.2.11 Fapi_issueAsyncCommand()
      12. 3.2.12 Fapi_checkFsmForReady()
      13. 3.2.13 Fapi_getFsmStatus()
    3. 3.3 Read Functions
      1. 3.3.1 Fapi_doBlankCheck()
      2. 3.3.2 Fapi_doVerify()
    4. 3.4 Informational Functions
      1. 3.4.1 Fapi_getLibraryInfo()
    5. 3.5 Utility Functions
      1. 3.5.1 Fapi_flushPipeline()
      2. 3.5.2 Fapi_calculateEcc()
      3. 3.5.3 Fapi_isAddressEcc()
      4. 3.5.4 Fapi_remapEccAddress()
      5. 3.5.5 Fapi_calculateFletcherChecksum()
  7. 4Recommended FSM Flows
    1. 4.1 New Devices From Factory
    2. 4.2 Recommended Erase Flow
    3. 4.3 Recommended Bank Erase Flow
    4. 4.4 Recommended Program Flow
  8. 5Software Application Assumptions of Use Related to Safety
  9.   A Flash State Machine Commands
  10.   B Typedefs, Defines, Enumerations and Structures
    1.     B.1 Type Definitions
    2.     B.2 Defines
    3.     B.3 Enumerations
      1.      B.3.1 Fapi_FlashProgrammingCommandsType
      2.      B.3.2 Fapi_FlashBankType
      3.      B.3.3 Fapi_FlashStateCommandsType
      4.      B.3.4 Fapi_StatusType
      5.      B.3.5 Fapi_ApiProductionStatusType
    4.     B.4 Structures
      1.      B.4.1 Fapi_FlashStatusWordType
      2.      B.4.2 Fapi_LibraryInfoType
  11.   C Summary of Changes for FAPI Library v5.00.00
  12.   D Revision History

Fapi_issueProgrammingCommandForEccAddresses()

Remaps an ECC address to data address and calls Fapi_issueProgrammingCommand().

Synopsis

Fapi_StatusType 
Fapi_issueProgrammingCommandForEccAddresses(
          uint32 *pu32StartAddress,
          uint16 *pu16EccBuffer,
          uint16   u16EccBufferSizeInBytes
                                           )

Parameters

pu32StartAddress [in] ECC start address in Flash for the ECC to be programmed
pu16EccBuffer [in] Pointer to the ECC buffer address
u16EccBufferSizeInBytes [in] Number of bytes in the ECC buffer
If the number of bytes is 1, LSB (ECC for lower 64 bits) gets programmed. MSB alone cannot be programmed using this function. If the number of bytes is 2, both LSB and MSB bytes of ECC get programmed.

Description

This function remaps an address in the ECC memory space to the corresponding data address space and then call Fapi_issueProgrammingCommand() to program the supplied ECC data. The same limitations for Fapi_issueProgrammingCommand() using Fapi_EccOnly mode applies to this function. The LSB of pu16EccBuffer corresponds to the lower 64 bits of the main array and the MSB of pu16EccBuffer corresponds to the upper 64 bits of the main array.

Note: The length of the pu16EccBuffer cannot exceed 2.
Note: This function does not check STATCMD after issuing the program command. The user application must check the STATCMD value when FSM has completed the program operation. STATCMD indicates if there is any failure occurrence during the program operation. The user application can use the Fapi_getFSMStatus function to obtain the STATCMD value.
Note: Fapi_EccOnly mode cannot be used for Bank0 DCSM OTP space. If used, an error is returned. For the DCSM OTP space, either Fapi_AutoEccGeneration or Fapi_DataAndEcc programming modes can be used.

Return Value

  • Fapi_Status_Success (success)
  • Fapi_Status_FsmBusy (FSM busy)
  • Fapi_Error_AsyncIncorrectEccBufferLength (failure: Data buffer size specified is incorrect)
  • Fapi_Error_FlashRegsNotWritable (failure: Flash register writes failed. The user can make sure that the API is executing from the same zone as that of the target address for flash operation OR the user can unlock before the flash operation.
Fapi_Error_InvalidAddress (failure: User provided an invalid address. For the valid address range, see the TMS320F28E12x Real-Tim Microcontrollers Data Manual for TMS320F28E12x.