SLVAE87B December 2020 – June 2025 BQ79600-Q1 , BQ79612-Q1 , BQ79614-Q1 , BQ79616-Q1 , BQ79652-Q1 , BQ79654-Q1 , BQ79656-Q1
Establish a clean grounding scheme to make sure of best performance of the device. There are three ground pins (AVSS, DVSS, CVSS) for the internal power supplies of the device and one ground reference (REFHM) for the precision reference. There are noisy grounds and quiet grounds that are separated in the layout initially and joint together in a lower PCB layer. The external components (for example, bypass capacitors) are tied to the proper grounding group if possible to keep the separation of noisy and quiet grounds apart.
Even on a PCB layer that is mainly for signal routing, a best practice to have as small an island of ground pour as possible to provide a low impedance ground, rather than simply by down the ground trace to an lower ground plane.
There is a strong recommendation to have a minimum of four layers in the PCB, with one fully dedicated as an unbroken VSS plane (except thermal reliefs). Avoid placing tracks on this layer to maintain the unbroken integrity of the plane structure.
If multiple devices are placed on the same PCB, then each device has a ground plane with proper layout clearance.
Figure 13-2 Separate Ground Plane per
Device on the Same PCB