SLVSHO1A March 2025 – December 2025 TPS1689
PRODUCTION DATA
BB_ERASE is a manufacturer specific command which fills the EEPROM Page-0 (where Blackbox information is stored) with all zeroes (0).
This command uses the PMBus® send byte protocol. There is no data byte for this command. This command is write only.
This command should be preceded by the MFR_WRITE_PROTECT command to unlock the device first to prevent accidental accidental/spurious writes. If the WP# pin is pulled low, the write access is completely disabled in hardware and MFR_WRITE_PROTECT command has no effect.