SLVSHS0B March 2025 – February 2026 TPS482H85-Q1
PRODUCTION DATA
When loss of GND occurs, all the channels are disabled regardless of control pin status, and the part is not powered.
Case 1 (loss of device GND): loss of GND protection is active when the thermal pad (Tab), IC_GND, and current limit ground are one trace connected to the system ground, as shown in Figure 7-15.
Case 2 (loss of module GND): when the whole ECU module GND is lost, protections are also active. At this condition, the load GND remains connected.