SLVUBT1A October   2019  – June 2020 TPS50601A-SP

 

  1.   TPS50601A-SP Worst Case Analysis Unencrypted PSpice Average Model User's Guide
    1.     Trademarks
    2. 1 TPS50601A-SP WCA Model Specification
    3. 2 Default Parameters
    4. 3 Example of using model with Cadence Pspice (17.2.0)
      1. 3.1 Creating a part from the netlist file
      2. 3.2 Steps to create project in Capture
      3. 3.3 Creating the schematic in Capture
    5. 4 Simulating the Model
      1. 4.1 Monte Carlo Analysis of Output Voltage
      2. 4.2 Frequency Response Analysis
        1. 4.2.1 Analyzing Frequency Response with Bode Plot
        2. 4.2.2 Analyzing Frequency Response with Histogram
  2.   Revision History

Steps to create project in Capture®

The following steps explain the procedure for creating a project in Capture and adding the part created from the netlist:

  1. Open the Capture application from Cadence - v17.2.0 or above.
  2. Click on File → New → Project.
  3. Enter a project name and location, choose PSpice Analog or Mixed A/D from the options, and click "OK".
  4. New_Project.png
  5. Once the Create Pspice Project dialogue box opens, select the "Create a blank project" option and click "OK".
  6. Setup5.png
  7. A new project will be created and the project window will open. Right click on the Library folder and select "Add File".
  8. Add_File.png
  9. Choose the ***.olb file that was previously created, add to the dialogue box, and click "Open". This will add the part symbol to the project.
  10. OLB.png