SLVUCP8A September 2024 – June 2025 TPS26750
J6 is a USB Type-C port that is configured as a 5V/3A legacy sink that provides a full speed USB connection to the EVM. J6 is used to interface with the GUI for part configuration and debug. For instructions on how to use the GUI, see Section 3.3.
This set of three connectors is intended to allow various power converter boards to interface with the TPS26750EVM.
The three connectors are listed below
The connectors are placed at a 600mil pitch between pin 1 of each connector. The generic power converter interface is on the right side of the board, as shown in Figure 1-1. The connectors for J9 are placed from bottom to top as follows (see schematic Figure 5-9, DC2DC Interface, for pinout):
| Pin Number | Signal |
|---|---|
| 1 (denoted by a white dot to the lower right of the pin) | PP5V |
| 2 | GND |
| 3 | GND |
| 4 | I2Cc_SCL |
| 5 | GPIO1 |
| 6 | I2Cc_SDA |
| 7 | GPIO3 |
| 8 | LDO_3V3 |