SLVUCP9B November 2023 – October 2025 TPS25751
After selecting the TPS25751 configuration, continue to fill out the remaining questions to flash or generate a full configuration. Based on the selection for Question 1, some of the remaining questions can be unavailable for selection.
Questions 2 through 4 asks for the maximum power that is sourced or sunk. If a source-only configuration is selected in Question 1, then Question 3 is not available to select. If a sink-only configuration is selected, then Question 2 is not available to select. Question 4 determines the power role preference of TPS25751, this question is only available if the system is DRP (Dual Role Power).
When selecting the maximum power that can be sourced or sink, this configures the Transmit Source Capabilities (0x32) and Transmit Sink Capabilities (0x33) register of TPS25751 by adding default Source/Sink PDOs. The voltage and current rating applies for both Source and Sink PDOs. See the figure below for the default configuration.
Question 5 asks for the supported USB speed. Based on the selection, this determines what USB speed is enumerated during PD negotiation. If USB data is not required, then select No USB data is being used.
Question 6 asks for the preferred data role. Based on the selection, this determines the data role (UFP, DFP, or DRP) TPS25751 is configured for. If there is no preference, then select No.
Question 7 asks for BC1.2 and legacy charging support. Based on the selection, TPS25751 can enumerate different BC1.2 charging schemes. Refer to the TPS25751 data sheet for more details.
Question 8 asks for Liquid Detection support. This is a new feature of TPS25751 based on the Type-C specifications for Liquid Detection and Corrosion Mitigation. Refer to Section 4.4 for more details.
Questions 9 and 10 asks for the Vendor ID and the desired Product ID respectively. The Vendor ID is given by the USB-IF and the Product ID is simply a configuration identifier. Select Yes option to enter 4-digit hexadecimal number, otherwise select No.
Questions 11 through 18 corresponds to configuring the selected BQ (Battery Charger) device if applicable. These questions are only available for filling in if a BQ configuration is selected in the first question. For all other non-BQ configuration (TPS25751 only), these questions are disabled. Refer to Section 4.3 section for more details on each questionnaire and the applications.