SLVUD17B February 2025 – November 2025 TPS65214
The NVM Configuration page does not require hardware to develop an NVM configuration. Connection with an actual device is needed only when attempting to upload to a target device.
Once the registers are set to the desired configuration, locate the File tab at the top of the screen and select a format for the configuration file (shown in Figure 3-10). Save the register configuration in a CSV (comma separated values), JSON (JavaScriptâ„¢ Object Notation), or TXT (plain text file) format. Next, use the Save Register Map option to download the saved configuration in the selected format.
To load an existing configuration into the NVM, use the Load Register Map option and locate configuration file. Save an existing register map, or download the Device OTP file from the OTP Validation tab for an example of the accepted format of the configuration file.
Figure 3-10 Save and Load Register
Options