The following sections outline
configuring the TPS65214EVM for general experimentation.
Configure the TPS65214EVM as
follows:
- Configure the regulator input
supply rails for the expected application using the jumpers indicated in the
Supply Voltage Setup.
- Configure the multifunction pins
externally using the mode configuration descriptions indicated in
Multi-Function pin setup. Please note that the default configuration
for regulator choice in SD or DDR voltage selection can differ for each
individual NVM configuration (polarity is configurable).
- Connect VSYS to a power supply
capable of supporting the application and enable the supply. Typical supply for
TPS6521401 is 5V.
- If using a version of TPS65214
configured for First Supply Detection (FSD), then the power-up sequence is
executed as soon as the 5V supply is connected to VSYS.