Use the following instructions to power up with ENABLE:
- Configure the jumper J1 position to the desired
slew rate as described in Jumper Descriptions and Default Positions.
- Set the input supply voltage VIN to 54V and current limit to 5A.
- Connect a capacitive load of 1mF between VOUT (connector T2) and PGND (connector T3).
- Connect the input supply between VIN (connector T1) and PGND (connector T3).
- Turn on the power supply by keeping the device disabled using the switch SW1.
- Enable the eFuses by releasing the switch SW1.
- Observe the waveform at VOUT (TP5) and input current using an oscilloscope to measure the slew rate and rise time of the VOUT with a given input voltage of 54V.
The start-up profile of TPS1689EVM with ENABLE
using two devices in parallel is shown in Figure 3-3.