SLVUDG9 September 2025
The Load from File button, shown in File Load Process, is used to load in a .csv file into the table. This can only be accessed once a device has been selected. Once the file dialog is opened, the user can select a .CSV file to load into the Memory Table.
Figure 2-13 File Load Process| Error | Explanation |
|---|---|
| Please select a device before loading from file | Device must be selected before populating table. Press Search Devices and then load from file. |
| Loaded csv file does not match memory map dimensions [col]/[row] | The loaded file contains a special character in a data cell, or the table loaded did not match the dimensions of the memory space of the device. Edit the CSV in a spreadsheet application and reload after fixing. Make sure CSV loaded was for the right type of memory. For example, BQ2026 files does not load for a TMF0008 device. |