SLVUDX5 June 2026
This section describes the connectors, test points, and jumpers on the EVM and how to properly connect, set up, and use the TPSM65660EVM. See Figure 2-3 for location of connectors and jumpers and typical setup.
| Signal | Connector and Test Points | Description |
|---|---|---|
| VIN | J1, TP1, VIN_S1 | The terminal block J1 is used as the input of the module. Apply input voltage between J1 and J2. TP1 and VIN_S1 can be used as positive DMM connection for VIN sensing. TP2 is used as the negative DMM connection for VOUT sensing. |
| VOUT | J3, TP3 | The terminal block J3 is used as the
output of the module. Connect the output load between J3 and J4. TP3 (S+) is used as the positive DMM connection for VOUT sensing. TP5 (S–) is used as the negative DMM connection for VOUT sensing. |
| GND | TP2, TP4, TP5 | Ground of the converter. TP4 can be used as any ground connector as needed. |
| EN | J5 | The EN jumper (J5) is used to enable
or disable the EVM. To use the external UVLO feature, populate R11 and R14 and remove the EN jumper shunt. Note that for accurate shutdown quiescent current measurement, these resistors must be removed (if used) and the EN jumper shunt moved to OFF. |
| MODE/SYNC | J6 | The MODE jumper (J6) is
used to select the operating mode. With MODE jumper removed, MODE pin in grounded
and device operates in the auto mode. The device operates in automatic PFM/FPWM mode
depending on load current. With MODE jumper installed, MODE pin is connected to VCC
and device operates in FPWM mode, the device operates at fixed frequency under all
load conditions. The MODE/SYNC pin is also the frequency synchronization input. To synchronize the device to an external clock, remove the MODE jumper shunt and apply the clock between the MODE/SYNC pin of J6 and GND |
| PGOOD | J12 | The PGOOD J12 is used to monitor the power-good indicator. This flag indicates whether the output voltage has reached the regulation level. PGOOD is an open-drain output that is tied to VCC through a 100kΩ resistor (R5) on the EVM. |
| FB Connections | J11 | The jumper J11 is used
to select the EVM output voltage setting. In the factory default configuration, the
EVM is configured for external adjustable setting for 12V output. Keep jumper open
for configuring in adjustable output voltage. Install jumper between FB Pin and VCC
for 5V fixed output and between FB and GND for 3.3V. Note: install R2 for fixed output configuration to close the loop. |
| CNFG/SYNCOUT | J7 | Resistor to GND for the primary device with external comp.
Short to VCC for Primary device with internal comp. Do not float if R12 is removed.
Note: for this EVM, while using external comp, remove two output caps. |
| BIAS | J8 | The BIAS Jumper (J8)
acts as an auxiliary input to the internal LDO regulator. C20 helps bypassing the
switching noise. In the EVM factory default configuration, BIAS is connected to VOUT
through R2. To change the LDO input to an available external supply from 3.3V to 30V, depopulate R2, and connect this pin to the external supply directly. If configured for fixed output voltage of 3.3V or 5V output, R2 must be installed to close the control loop. See also the TPSM65660 datasheet. |
| Loop response plot | J13, TP4 | When using the
adjustable output voltage mode, a Bode plot measurement can be taken using the
connection shown in Figure 2-4. R3 must be populated for this test, and probes must have a ground connection to
TP4. In the fixed 3.3V or 5V output voltage configuration, a Bode plot measurement cannot be taken. TI suggests to run a step load response to evaluate the loop stability. |
| DRSS/MCOMM | J9, J10 | Dual Random Spread-Spectrum (DRSS) select pin. See also Table 2-1 for available DRSS options. If configured for dual-phase operation, this pin becomes a mode communication pin between a primary and a secondary device. For dual-phase operation, tie together the MCOMM pins of the primary and secondary devices. |
| DRSS/MCOMM Pin | DRSS | Slew Rate Control |
|---|---|---|
| Short to VCC | Enabled, ±10%, 6kHz | Enabled |
| Float | Enabled, ±10%, 6kHz | Enabled |
| 150kΩ to PGND | Enabled, ±10%, 6kHz | Disabled |
| 49.9kΩ to PGND | Disabled | Disabled |
| Short to PGND | Disabled | Disabled |