SLYY234 December 2024 AMC0106M05 , AMC0106M25 , AMC0136 , AMC0311D , AMC0311S , AMC0386 , AMC0386-Q1 , AMC1100 , AMC1106M05 , AMC1200 , AMC1200-Q1 , AMC1202 , AMC1203 , AMC1204 , AMC1211-Q1 , AMC1300 , AMC1300B-Q1 , AMC1301 , AMC1301-Q1 , AMC1302-Q1 , AMC1303M2510 , AMC1304L25 , AMC1304M25 , AMC1305M25 , AMC1305M25-Q1 , AMC1306M05 , AMC1306M25 , AMC1311 , AMC1311-Q1 , AMC131M03 , AMC1336 , AMC1336-Q1 , AMC1350 , AMC1350-Q1 , AMC23C12 , AMC3301 , AMC3330 , AMC3330-Q1
The last method for clock signal compensation is clock inversion at the MCU and works for Delta-Sigma modulators with external and internal clock source. In that case, the selected MCU must be capable of inverting the GPIO input. The TMS320F28379D GPIO inputs prior to the SDFM (Sigma Delta Filter Module) can be configured to invert the input signal at any GPIO, as shown in Figure 154. For example, the clock input signal is inverted at GPIO123, hence the SD1_C1 clock signal is inverted versus the AMC1303Mx clock signal. As a result, the SDFM samples the input data SD1_D1 versus the falling edge of the external clock signal at the input of GPIO123, as shown in Figure 155.
By inverting the clock input signal by using the GPIO a fixed delay of one-half of the clock period is added to the clock signal. Depending on the timing specifications and propagation delays of the system setup, this additional delay may be sufficient to meet the TMS320F28379D setup and hold timings of minimum 10 ns for the SDFM qualified GPIO (3-sample) mode 0. However, as this clock signal compensation method’s additional delay time is fixed and cannot be changed, it must be verified for each system design that the resulting timings for setup and hold of the MCU for the SDFM qualified GPIO (3-sample) mode 0 are met.
This compensation method is also applicable to Sitara MCUs, where both the rising and falling edges of the external clock signal can be set as data acquisition point by software.