SNAS871A July 2025 – February 2026 LMR60406-Q1
PRODMIX
The LMR60406-Q1 device can be configured to operate in either fixed or adjustable output voltage modes. For fixed output voltages as specified by the device orderable part number, simply connect the output voltage rail directly to the FB pin. When other output voltages are required, a resistor divider between the output voltage rail and ground with the FB pin as the center point set the output. Use Equation 13 to calculate the output voltage given a specific feedback divider.
Alternatively, if the output voltage and RFBT are already known, use Equation 14 to calculate the value of RFBB.
Note that typically 100kΩ is used for RFBT.