SNAU265D June   2021  – February 2025 HDC3020 , HDC3020-Q1 , HDC3021 , HDC3021-Q1 , HDC3022 , HDC3022-Q1 , HDC3120 , HDC3120-Q1

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1HDC3x Devices
    1. 1.1 HDC3x2x Package Comparison
    2. 1.2 HDC3020 in WSON
    3. 1.3 HDC3021 in WSON
    4. 1.4 HDC3022 in WSON
    5.     HDC3120 in WSON
  5. 2Storage and Handling Guidelines
    1. 2.1 Exposure to Contaminants
    2. 2.2 Chemical Analysis
      1. 2.2.1 Saturation and Recovery Tests
      2. 2.2.2 Long-Term Exposure
    3. 2.3 Packaging and Storing
      1. 2.3.1 Assembly
      2. 2.3.2 Application in Extreme Environment
  6. 3Programming the HDC3020
    1. 3.1 The Functional Modes
    2. 3.2 Trigger-On Demand
    3. 3.3 Auto Measurement
    4. 3.4 Programming the CRC
      1. 3.4.1 CRC C Code
    5. 3.5 Example Code
    6. 3.6 Condensation Removal
    7. 3.7 Offset Error Correction
      1. 3.7.1 Offset Error Correction Example With a Fingerboard
  7. 4References
  8. 5Revision History

Saturation and Recovery Tests

The chemicals in this list were exposed to the sensor only for a short period of time. Two conditions were evaluated for each chemical: a 30-second exposure and eight 30-second exposures over a period of 24 hours.

Table 2-1 shows the chemicals in this list. The device operated at 3.3V at 30°C and an average humidity error was calculated.

Table 2-1 List of Chemicals for the Short-Term Exposure Test
Chemical Concentration Observable Damage Number of HDC3020 Units
Isopropyl alcohol 65.7% m/m None 4 per exposure rating
Hydrogen Peroxide 7.35% m/m None
Sodium Hypochlorite 4.5% m/m Copper traces corroded
Iodophors 74 ppm m/m None
Flux - Microcare Universal Contact Cleaner 100% None

30-Second exposure: Five drops of each chemical was dropped directly on the sensor opening. After 30 seconds, the sensor was turned over to get rid of excess solution. After a minute of exposure, the device was cleaned to prevent further exposure.

Overall, Figure 2-1 shows there is not much change between the pre- and post tests for these chemicals other than a small negative gain.

HDC3020 Short-Term Exposure: One-Time
          Exposure Figure 2-1 Short-Term Exposure: One-Time Exposure

Multiple 30-second exposures: Four HDC3020 devices followed a similar procedure as the 30-second test. The procedure was performed seven more times.

Overall, most of the chemicals did not have any major shift other than a negative gain.

However, exposure to Sodium Hypochlorite resulted in some corrosion on the copper traces on the board and some of the pins. To clean the PCB, the opening was protected using a kapton cover and it was cleaned using a horsehair brush and DI water. A humidity sweep shows that the devices had a very large negative gain shift, especially at higher humidity setpoints.

Exposure to Isopropyl Alcohol also resulted in some negative gain shift at lower humidity setpoints. Any further exposure would result to severe gain shifts.

Figure 2-2 shows the sweeps for this exposure.

HDC3020 Short-Term Exposure: Multiple
          Exposures Figure 2-2 Short-Term Exposure: Multiple Exposures