SNAU283 October 2022
Click Default configuration → CLKin1 122.88 MHz, OSCin 122.88 MHz, VCO1 2949.12 MHz. Press Ctrl+L to restore the default configuration.
Figure 5-3 Setting the Default
Configuration for LMK04368-EP. For the purpose of this walkthrough, a default mode will be loaded to ensure a common starting point. This is important because when TICS Pro is closed, the software remembers the last settings used for a particular device. Again, remember to press Ctrl+L as the first step after loading a default mode.