SNAU297 July 2025 LMK5B12212 , LMK5C22212A
In Step 2, set up the clock input frequencies, interface types, and the frequency accuracies (ppm).
The ppm errors of XO and REFx are used to calculate the frequency validation according to the selected parameter located on the right side of this step.
Figure 3-4 Step 1 and 2: XO Input and Clock
Inputs