SNAU297 July 2025 LMK5B12212 , LMK5C22212A
The Outputs page shows all the possible source frequencies to the output channels. To simplify settings fields necessary to providing an output frequency, a source mux lists all possible sources for each output. Be sure to enable or disable the desired outputs on the right-hand side of the screen.
There are many detailed output pages beneath the Outputs page that show the individual controls for each set of outputs.
The black line between OUT2 to OUT3, OUT4 to OUT7, and OUT8 to OUT11 signifies that all these outputs must source from the same VCO.
Figure 3-23 Outputs Page