SNAU318 June 2025 LMX1205
The input and output path clock have individually programmable delays. The clock signal delay is up to 60ps, with 1.1ps resolution per code from the input path and 55ps with 0.9ps resolution per code at the output path. To highlight the feature, skew an output clock (CLKOUT1) channel trace by approximately 10ps in secondary1 device with respect to CLKOUT2 of the same device. CLKOUT2 of secondary 2 device is skewed by approximately 5ps with respect to CLKOUT1 of the same device. The secondary 2 device skew allows the user to validate the programmable delay feature offered by the device.
Figure 4-10 Clock Out Path with Trace
Length SkewedFigure 4-11 shows the waveform plot of the secondary1 device. Figure 4-11 shows a 10.8ps skew from other channels.
Figure 4-11 Channel to Channel Skew of
Clock Path with Trace length mismatchTo skew the waveform:
Figure 4-12 Software Configuration
for Device Selection
Figure 4-13 Software Configuration for
changing Clock Path Output DelayFigure 4-14 shows the waveform after adjusting the output delay so that the channel-to-channel skew is < 1ps.
Figure 4-14 Channel to Channel Skew After
Adjusting the Output Delay of the Clock PathThe programmable delay feature of the device has wide range of applications. One application of the delay features is to calibrate and adjust the output delays of clock path to align all clock output edges in a large phased array cascaded clock tree. Another application is to offset a mismatch in:
The delay features also uses windowing to align the SYSREF edges to the clock falling edge.