SNIU028E February 2016 – February 2025 UCD3138 , UCD3138064 , UCD3138064A , UCD3138128 , UCD3138A , UCD3138A64
If a PMBus message to the UCD is halted in the middle of a byte, the UCD bit counter may not be reset to zero. Therefore the UCD may not respond correctly to the next message. Normally the bit counter will be resychronized after this one incorrect response, so subsequent messages will be handled correctly.
On the UCD3138, and UCD3138064, this is the case. On the UCD3138A64 and UCD3138128 and all A versions, stopping the message in the middle of the byte should be handled correctly.