SNIU028E February 2016 – February 2025 UCD3138 , UCD3138064 , UCD3138064A , UCD3138128 , UCD3138A , UCD3138A64
The 16PWMx timers have a 16 bit counter driven by a prescaler, which is driven by ICLK. They have 2 compare units which combine to control one output pin. Each compare unit can generate an interrupt, as can the counter overflow. All of the interrupts from a specific timer are combined into one before being sent to the CIM interrupt module. Each timer has its own interrupt bit in the CIM.
Figure 11-2