SNIU028E February 2016 – February 2025 UCD3138 , UCD3138064 , UCD3138064A , UCD3138128 , UCD3138A , UCD3138A64
The UART receiver and transmitter can be controlled by interrupts. The receive and transmit interrupts allow efficient operation of the UART by reading and writing character information to and from the UART as new data arrives and when old data has just been sent.
The RXRDY flag (UARTRXST.2) used by the receiver indicates that new data is available to be read.
The receiver also has various error interrupts that indicate when a particular error condition is active. An active error interrupt condition is indicated by the RXERR flag in UARTRXST.
However, the exact source of an error interrupt can be determined by checking the parity error (PE), frame error (FE), overrun error (OE), break-detect (BRKDT), and wake-up (WAKEUP) flags also located in UARTRXST.
Additionally, the transmitter uses the TXRDY flag (UARTTXST.2) to indicate that the transmitter is ready for new data to be written that will be sent to the bus.
Transmit, receive, and error interrupts are enabled or disabled through separate interrupt-enable bits. When not enabled, the interrupts are not asserted; however, polled operation of the UART is still possible because the interrupt flags continue to indicate module events.
The UART module generates three interrupt requests to the UCD3138 system module: one each for transmitter, receiver, and error interrupts. Each of these interrupts must also be configured in the UCD3138 system module before operation.
Normally, the error interrupt has the highest priority, the receiver interrupt has the next highest priority, and the transmitter generally has the lowest priority.
This prioritizing scheme reduces the possibility of missed error conditions and receiver overrun. For interrupt priority levels on a specific device, consult the UCD3138 device datasheet.