SNLS647I December 2019 – August 2025 DP83826E , DP83826I
PRODUCTION DATA
The ENHANCED mode is one of two modes that the DP83826 can be configured in at start-up. This mode allows the DP83826 to support real-time Ethernet applications in addition to the standard Ethernet applications. To configure the DP83826 to ENHANCED mode, leave ModeSelect (pin 1) unconnected or pull up with a resistor to VDDIO.
| PIN | TYPE (1) | DESCRIPTION | |
|---|---|---|---|
| NAME | NO | ||
| ModeSelect | 1 | Reset: I, PU Active: I, PU | This pin selects the DP83826 operating mode: BASIC mode or ENHANCED mode. For ENHANCED mode, this pin shall be left NC or pulled-up with a resistor to VDDIO. For BASIC mode, this pin shall be shorted to GND. |
| CEXT | 2 | A | External capacitor: Connect the CEXT pin through a 2nF capacitor to GND. |
| VDDA3V3 | 3 | Power | Input analog supply: 3.3V. For decoupling capacitor requirements, refer to Power Supply Recommendations section of data sheet. |
| RD_M | 4 | A | Differential receive input (physical media dependent: PMD): These differential inputs are automatically configured to accept either 10BASE-Te, 100BASE-TX specific signaling mode. |
| RD_P | 5 | A | |
| TD_M | 6 | A | Differential transmit output (PMD): These differential outputs are configured to either 10BASE-Te or 100BASE-TX signaling mode based on configuration chosen for PHY. |
| TD_P | 7 | A | |
| XO | 8 | A | Crystal output: Reference clock output. XO pin is used for crystal only. Leave this pin floating when a CMOS-level oscillator is connected to XI. |
| XI/50MHzIn | 9 | A | Crystal or oscillator input clock: MII mode, RMII leader mode: 25MHz ± 50ppm tolerance crystal or oscillator clock. RMII follower mode: 50MHz ± 50ppm tolerance CMOS-level oscillator clock. |
| RBIAS | 10 | A | RBIAS ( Bias resistor) value 6.49kΩ with 1% precision connected to ground. |
| MDIO | 11 | Reset: I, PU Active: I/O, PU | Management data I/O: Bi-directional management data signal that can be sourced by the management station or the PHY. This pin has internal pullup resistor of 10kΩ. An external pullup resistor can be added if needed. |
| MDC | 12 | Reset: I, PD Active: I, PD | Management data clock: Synchronous clock to the MDIO serial management input/output data. This clock can be asynchronous to the MAC transmit and receive clocks. The maximum clock rate is 25MHz. There is no minimum clock rate. |
| RX_D3 | 13 | Reset: I, PD Active: O Strap7 | Receive data: Symbols received on the cable are decoded and presented on these pins synchronous to the rising edge of RX_CLK and contain valid data when RX_DV is asserted. A nibble RX_D[3:0] is received in MII mode. 2-bits RX_D[1:0] is received in RMII mode. |
| RX_D2 | 14 | Reset: I, PD Active: O Strap8 | |
| RX_D1 | 15 | Reset: I, PD Active: O Strap9 | |
| RX_D0 | 16 | Reset: I, PD Active: O Strap0 | |
| VDDIO | 17 | Power | I/O supply voltage: 3.3V or 1.8V. For decoupling capacitor requirements, refer to Power Supply Decoupling Recommendations section of data sheet. |
| RX_DV/ CRS_DV | 18 | Reset: I, PD Active: O Strap10 | Receive data valid: This pin indicates valid data is present on the RX_D[3:0] for MII mode and on RX_D[1:0] in RMII mode. In MII mode, this pin acts as RX_DV. In RMII mode, this pin acts as CRS_DV and combines the RMII Carrier and Receive Data Valid indications. This pin can be configured to RX_DV in RMII mode to enable RMII Repeater Mode. |
| RX_CLK/ 50MHz_RMII | 19 | Reset: I, PD Active: O | MII receive clock: MII Receive Clock provides a 25MHz
reference clock for 100bps speed and a 2.5MHz reference clock for
10Mbps speed, which is derived from the received data stream. In RMII leader mode, this provides 50MHz reference clock. In RMII follower mode, this pin is not used and remains Input, pulldown. |
| RX_ER | 20 | Reset: I, PD Active: O Strap6 | Receive error: This pin indicates that an error symbol has been detected within a received packet in both MII and RMII mode. In MII mode, RX_ER is asserted high synchronously to the rising edge of RX_CLK. In RMII mode, RX_ER is asserted high synchronously to the rising edge of the reference clock. RX_ER is asserted high for every reception error, including errors during Idle. This strap only latches on power-up and not on pin reset. |
| PWRDN/INT | 21 | Reset: I, PU Active: I/O, PU | Power down (default), interrupt: The default function of this pin is power down. Register access is required to configure this pin as an interrupt. In power down function, an active low signal on this pin places the device in power down mode. When this pin is configured as an interrupt pin, this pin is asserted low when an interrupt condition occurs. The pin has an open-drain output with a weak internal pullup resistor (9.5kΩ). Some applications require an external PU resistor. |
| TX_CLK | 22 | Reset: I, PD Active: O Strap5 | MII transmit clock: MII transmit clock provides a 25MHz reference clock for 100Mbps speed and a 2.5MHz reference clock for 10Mbps speed. Note that in MII mode, this clock has constant phase referenced to the input clock. Unused in RMII Mode. |
| TX_EN | 23 | Reset: I, PD Active: I, PD | Transmit enable: TX_EN is presented on the rising edge of the TX_CLK. TX_EN indicates the presence of valid data inputs on TX_D[3:0] in MII mode and on TX_D[1:0] in RMII mode. TX_EN is an active high signal. |
| TX_D0 | 24 | Reset: I, PD Active: I, PD | Transmit data: In MII mode, the transmit data nibble received from the MAC is synchronous to the rising edge of TX_CLK. In RMII mode, TX_D[1:0] received from the MAC is synchronous to the rising edge of the reference clock. |
| TX_D1 | 25 | Reset: I, PD Active: I, PD | |
| TX_D2 | 26 | Reset: I, PD Active: I, PD | |
| TX_D3 | 27 | Reset: I, PD Active: I, PD | |
| COL/LED2/TX_ER/GPIO | 28 | Reset: I, PD Active: O Strap4 | Collision Detect (default): In MII mode when the pin is acting as Collision Detect (COL), this pin is always LOW in Full Duplex mode. In Half Duplex mode, COL is asserted HIGH only when both transmit and receive media are non-idle. This pin can also be configured as a second additional LED driver (LED2), the MII TX_ER signal or general purpose I/O (GPIO) through register configurations. In RMII mode, this pin acts as LED2 by default. |
| CRS/LED3 | 29 | Reset: I, PD Active: O Strap3 | Carrier sense (default): In MII mode this pin is asserted high when the receive or transmit medium is non-idle. Carrier sense and receive data valid. This pin can be configured as third LED (LED3) through register configuration. In RMII mode, this pin is configured as LED3 by default. |
| LED0 | 30 | Reset: I, PD Active: O Strap2 | LED0: This LED indicates transmit and receive activity in addition to the status of the Link. The LED is ON when link is good. The LED blinks when the transmitter or receiver is active. LED polarity is auto-detected (Active Low/ Active High) based on external pull-up or pull-down on the pin. |
| CLKOUT/ LED1 | 31 | Reset: I, PU Active: O Strap1 | This pin provides 25MHz reference clock from XI as default
output after power-on reset (POR). The output is not affected by
Resets allowing Application to reset PHY without impacting other
system getting impacted. The output clock switches off only by Deep
Power Down. The pin can be configured to act as LED1 using strap or register configuration. The strap only latches on power-up and not on pin reset. The LED is ON when link is 100Mbps. LED remains OFF if Link is 10Mbps or no Link. LED polarity is auto-detected (Active Low/ Active High) based on external pull-up or pull-down on the pin. This strap only latches on power-up and not on pin reset. |
| RST_N | 32 | Reset: I, PU Active: I, PU | Reset low: RST_N pin is an active low reset input. Asserting this pin low for at least 25μs forces a reset process to occur. Initiation of reset causes strap pins to be re-scanned and resets all the internal registers of the PHY to default value. |