SNLU237B September 2018 – July 2025 DP83869HM
Download the software from http://www.ti.com/tool/usb-2-mdio. The Web page also contains a User’s Guide for installing and using the software.
The MSP430 is on board the EVM, so the user does not have to purchase a separate MSP430 Launchpad kit and connect to the PHY using wires. The entire EVM can be powered and controlled through a USB connector. MSP430 and USB2MDIO utility can be used even when power is not supplied through a USB.
In case the onboard MSP430 cannot be used due to some reason, MDIO and MDC pins are also broken out on the J15 connector. Customers can connect a MSP430 launchpad or their own MDIO-MDC utility on J15 to access the PHY registers.