SNOSDL9A December 2024 – December 2025 LMG5126
PRODUCTION DATA
Input capacitors are always required to provide a stable input voltage. It is necessary that the input capacitors is able to handle the inductor ripple current.
The single phase boost input RMS ripple current is expressed as,
The input capacitor is also an important part of the input filter. Higher capacitance and ESR help damping the input filter better. Aluminum electrolytic capacitor is a good choice for input capacitor with high capacitance and ESR. Refer to Input Filter Design for Switching Power Supplies application note for more details.