SNVA991 October 2022 LM5123-Q1
The output capacitor is required to smooth the load voltage ripple, provides an energy source during load transients. The output capacitor bank and the control loop bandwidth impact the dynamic load transient response of the regulator. The output capacitor delivers energy to the load until the control loop can adjust to the new operating point. The control loop crossover frequency is estimated to approximately 1/8 the right-half plan zero of the boost plant transfer function using Equation 11.
The estimated control loop crossover frequency estimated to be 2.45 kHz. Note that the minimum right-half plane zero frequency occurs at the minimum input voltage and maximum output power.
With the target crossover frequency selected, the minimum output capacitance is calculated based on the transient response for a given loaded step using Equation 12. In a variable output voltage design the maximum load step occurs at the minimum target load voltage and the output capacitance is sized accordingly.
where
The calculated output capacitance is 752 μF, and for this design is selected to be 900 μF.
The output capacitor must be rated to handle the RMS current during the off time of the low-side switch. The maximum output ripple current is estimated using Equation 13.
where
The estimated RMS current of the output capacitor bank is 11.82 A. Note the highest output capacitor RMS current occurs at the worst case operating condition, minimum supply voltage, maximum load voltage and full power. The output capacitor bank is comprised of both electrolytic capacitors and ceramic capacitors. Each chemistry benefits the design. Electrolytic capacitors provide a large bulk capacitance for low frequency energy storage to handle load transient demands, in a relatively small footprint. Ceramic capacitors provide a low ESR and low ESL decoupling path to minimize switching noise being coupled to the load voltage. Ceramic capacitor typically has very high RMS current rating. Due to the benefits of each chemistry the output capacitor bank is comprised of both electrolytic and ceramic capacitors.