SNVA991 October 2022 LM5123-Q1
The RCOMP resistor and CCOMP capacitor set the zero frequency of the compensation network. The zero of the compensation network provides a phase boost to stabilize the control loop. To provide adequate phase margin the zero frequency is placed at the geometric mean of the crossover frequency (fCROSS) and the low frequency pole of the plant (fPlf). The low frequency pole of the modulator and the zero frequency of the compensation network are estimated using Equation 24and Equation 25, respectively
The the zero frequency of the compensation network estimated to be approximately 373 Hz. Knowing the target frequency, CCOMP is calculate using Equation 26.
CCOMP is calculated to be 7.7 nF. Selecting the nearest standard value CCOMP is selected to be 6.8 nF.