SNVA991A October 2022 – October 2025 LM5123-Q1
The inductance value of the boost regulator is calculated with respect to the inductor current ripple ratio (RR). The ripple ratio is defined as the peak to peak ripple current over the average inductor current. In a boost topology the average inductor current is equal to the average input current. There are three main considerations guiding the selection of the inductance value: the inductor power loss, the falling slope of the inductor current and the right-half plane (RHP) zero frequency (ωZ_RHP) of the control loop.
A maximum ripple ratio between 30% and 60% yields a balanced compromise among the above considerations. In this example, the maximum ripple ratio of the inductor current is selected to be 60%. The ripple ratio is calculated at the maximum output voltage (VLOADmax) and maximum output power (POUTmax) to properly select the inductance value. In continuous conduction mode the duty cycle is estimated using Equation 2. The ripple ratio is calculated using Equation 3.
where
Locating the operating point at which the maximum ripple ratio is dependent on the duty cycle range. In CCM operation the maximum ripple ratio typically occurs at 33% duty cycle. When the duty cycle at the maximum input voltage is greater than 33% the maximum ripple ratio occurs at VSUPPLYmax. When the duty cycle at the minimum input voltage is less than 33% the maximum ripple ratio occurs at VSUPPLYmin.
Leveraging Equation 2, the duty cycle at the maximum input voltage is calculated to be 48.6% when the output voltage is set to VLOADmax. The maximum ripple ratio occurs when VSUPPLY is at the maximum specified value. If the design operates at 33% duty, Equation 4 is used to back calculate the supply voltage at given duty cycle.
where
For this design example VSUPPLY_ΔILmax is equal to 18 V. Knowing maximum ripple ratio operating point, the desired ripple ratio, load current and the switching frequency, the inductance is calculated using Equation 5
A standard inductance of 2.6 µH is selected to satisfy the design criteria.
The maximum peak inductor current occurs at the minimum supply voltage, VSUPPLY_min, and the maximum load current ILOADmax. The peak inductor current is the sum of the average input current and half of the inductor peak-peak ripple, and is calculated using Equation 6.