SNVSBR8E March 2020 – October 2025 LMQ61460
PRODUCTION DATA
The device uses a reference-based soft start that prevents output voltage overshoots and large inrush currents during start-up. Soft start is triggered by any of the following conditions:
After soft start is triggered, the IC takes the following actions:
Together, these actions provide start-up with limited inrush currents and also allow the use of larger output capacitors and higher loading conditions that cause current to border on current limit during start-up without triggering hiccup. See Figure 7-8.

Any time the output voltage falls more than a few percent, the output voltage ramps up slowly. This condition is called recovery from dropout and differs from soft start in three important ways:
Despite being called recovery from dropout, this feature is active whenever output voltage drops to a few percent lower than the set point, which primarily occurs under the following conditions:

Figure 7-10 Recovery From Dropout (VOUT = 5 V, IOUT = 4 A, VIN = 13.5 V to 4 V to 13.5 V)