SNVSBR8E March 2020 – October 2025 LMQ61460
PRODUCTION DATA
The device can have two behaviors while lightly loaded. One behavior, called auto mode operation, allows for seamless transition between normal current mode operation while heavily loaded and highly efficient light load operation. The other behavior, called FPWM mode, maintains full frequency even when unloaded. Which mode the device operates in depends on which factory option is employed, see Section 4. Note that all parts operate in FPWM mode when synchronizing frequency to an external signal.
In auto mode, light load operation is employed in the device at load lower than approximately a tenth of the rated maximum output current. Light-load operation employs two techniques to improve efficiency:
Note that while these two features operate together to create excellent light load behavior, they operate independently of each other.