SNVU932A March 2025 – August 2025 LP5814 , LP5814I , LP5815
This section shows the steps to turn on the red LED (OUT2) and white LED (OUT3) LEDs in autonomous animation mode with the patterns as shown in Table 3-1 and .
| LED | PATTERNS |
|---|---|
| Red LED (OUT2) |
Animation Mode, Blinking with 5Hz Frequency |
| White LED (OUT3) | Animation Mode, Breathing with 1s Exponential Ramping Up and 1s Exponential Ramping Down |
Enable chip through clicking Chip Enabled button as shown in Figure 3-15.
Select the red LED (OUT2) and white LED (OUT3) to do the configuration through clicking the red LED and white LED with Shift keyboard button pushed.
Enable the selected red LED and white LED through selecting the Enable item from the Enable LED pulldown menu.
Set the selected red LED and white LED in autonomous animation mode through selecting the Auto item from the Select Mode pulldown menu.
Enable exponential PWM dimming for the selected red LED and white LED through selecting the Exponential item from the PWM Dimming Scale pulldown menu.
Click the Auto Mode Configuration tab to open the patterns setting panel as shown in Figure 3-17.
Select engine 0 for selected red LED (OUT2) through selecting the Engine0 is selected item from the OUT2 Engine Channel pulldown menu.
Select engine 1 for selected white LED (OUT3) through selecting the Engine1 is selected item from the OUT3 Engine Channel pulldown menu
Enable engine 0 order 0 through clicking the toggle button besides the Order 0 under Engine 0 control panel. Select pattern 0 for engine 0 order 0 through selecting the Pattern0 is selected item from the pulldown menu under the Order 0 as shown in Figure 3-18.
Enable engine 1 order 0 through clicking the toggle button besides the Order 0 under Engine 1 control panel. Select pattern 1 for engine 1 order 0 through selecting the Pattern1 is selected item from the pulldown menu under the Order 0 as shown in Figure 3-18.
Set the parameters of pattern 0 as the value shown in the Table 3-2 table.
Set the parameters of pattern 1 as the value shown in the Table 3-3 table.
Enter the values under the PATTERN 0 and PATTERN 1 control panels as shown in Figure 3-19.
| Address | Register | Set Value | Description |
|---|---|---|---|
| 1Ch | PATTERN0_PAUSE_TIME | 00h | No pause time |
| 1Dh | PATTERN0_REPEAT_TIME | 0Fh | Infinite repeat times |
| 1Eh | PATTERN0_PWM0 | FFh | PATTERN0_PWM0 = FFh |
| 1Fh | PATTERN0_PWM1 | FFh | PATTERN0_PWM1 = FFh |
| 20h | PATTERN0_PWM2 | 00h | PATTERN0_PWM2 = 0 |
| 21h | PATTERN0_PWM3 | 00h | PATTERN0_PWM3 = 0 |
| 22h | PATTERN0_PWM4 | 00h | PATTERN0_PWM4 = 0 |
| 23h | PATTERN0_SLOPER_TIME1 | 02h | PATTERN0_SLOPER_T1 = 0, PATTERN0_SLOPER_T0 = 0.1s |
| 24h | PATTERN0_SLOPER_TIME2 | 02h | PATTERN0_SLOPER_T3 = 0, PATTERN0_SLOPER_T2 = 0.1s |
| Address | Register | Set Value | Description |
|---|---|---|---|
| 25h | PATTERN1_PAUSE_TIME | 00h | No pause time |
| 26h | PATTERN1_REPEAT_TIME | 0Fh | Infinite repeat times |
| 27h | PATTERN1_PWM0 | 00h | PATTERN1_PWM0 = 0 |
| 28h | PATTERN1_PWM1 | FFh | PATTERN1_PWM1 = FFh |
| 29h | PATTERN1_PWM2 | FFh | PATTERN1_PWM2 = FFh |
| 2Ah | PATTERN1_PWM3 | 00h | PATTERN1_PWM3 = 0 |
| 2Bh | PATTERN1_PWM4 | 00h | PATTERN1_PWM4 = 0 |
| 2Ch | PATTERN1_SLOPER_TIME1 | 4Bh | PATTERN1_SLOPER_T1 = 0.2s, PATTERN1_SLOPER_T0 = 1s |
| 2Dh | PATTERN1_SLOPER_TIME2 | 4Bh | PATTERN1_SLOPER_T3 = 0.2s, PATTERN1_SLOPER_T2 = 1s |
The selected red LED starts blinking in 5Hz frequency and selected white LED starts breathing up and down after sending start command.