SNVU932A March 2025 – August 2025 LP5814 , LP5814I , LP5815
The LP581x_RUKA GUI software is downloaded from the link: LP581x_RUKA GUI.
On the Gallery page as shown in Figure 3-1, click the blank part of the panel to open the online version or click the Download button and select the platform to install the offline version to the user's computer.
For the offline version, after the download completed, extract the file and double click the exe application file to start the installation. Then follow the setup wizard to complete the installation, during which the license has to be accepted and all the default settings are kept. The installation takes about several ten minutes depends on the network speed.
Figure 3-2 appears to prompt that the offline version is installed successfully. Click the Finish button to start the GUI evaluation.