When a legacy product only contains a serial port for configuration or control, continuing to access the legacy product through the serial interface can become challenging over time. The following are the challenges of using a serial port:
Using Ethernet in place of the serial port provides the following benefits:
The software described in this application report (enet_s2e) allows an Ethernet-enabled TM4C129x microcontroller to be used as a serial-to-Ethernet converter. By connecting a serial-to-Ethernet converter to the serial port of a legacy product, it can be given the ability to operate on the Ethernet without requiring any changes to the existing hardware or software. This is especially useful when the legacy product cannot be modified (such as in the case of third-party products).
The software works out of the box on an EK-TM4C1294XL board. With minor modifications, the software can run on the DK-TM4C129X board. For details, see Section 3.2.
FreeRTOS has been used for scheduling the various tasks. Although an RTOS is not a requirement for this application, it has been used to make the application easily scalable.