SPNA248 March 2021 TM4C1292NCPDT , TM4C1292NCPDT , TM4C1292NCZAD , TM4C1292NCZAD , TM4C1294KCPDT , TM4C1294KCPDT , TM4C1294NCPDT , TM4C1294NCPDT , TM4C1294NCZAD , TM4C1294NCZAD , TM4C1299KCZAD , TM4C1299KCZAD , TM4C1299NCZAD , TM4C1299NCZAD , TM4C129DNCPDT , TM4C129DNCPDT , TM4C129DNCZAD , TM4C129DNCZAD , TM4C129EKCPDT , TM4C129EKCPDT , TM4C129ENCPDT , TM4C129ENCPDT , TM4C129ENCZAD , TM4C129ENCZAD , TM4C129LNCZAD , TM4C129LNCZAD , TM4C129XKCZAD , TM4C129XKCZAD , TM4C129XNCZAD , TM4C129XNCZAD
For more information on how to setup the SocketTest for UDP testing, see Section 7.1. The SocketTest in Figure 12-1 shows the two messages sent and received by the server. The length of the two messages is displayed in the terminal window. You can cross-reference the messages captured by Wireshark in Figure 12-2. First, the greetings message is sent. Then the two echo messages, with their received lengths, are sent by the client.
Figure 12-1 Enet_udpecho_client_lwip Output
Figure 12-2 Client Server Wireshark Capture for Enet_udpecho_client_lwip