SPRAD51A December 2023 – April 2024 F29H850TU , F29H859TU-Q1 , TMS320F2800157 , TMS320F280039 , TMS320F280039-Q1 , TMS320F280039C , TMS320F280039C-Q1 , TMS320F28P659DK-Q1
can_flash_programmer.exe –d f28003x –k <flash_kernel.txt> -a <file>This first loads the flash_kernel into RAM of the device using the bootloader. Then, the kernel executes and loads and programs flash with the file specified by the ‘-a’ command line argument, as seen in and .
This automatically connects to the device, performs an auto baud lock, downloads the CPU1 kernel into RAM and executes it. Now, the CPU1 kernel is running and waiting for a packet from the host.
Figure 6-4 CAN Flash Programmer Prompt After Downloading Flash Kernel to RAM
Figure 6-5 CAN Flash Programmer After Downloading Flash Application