SPRAD86 March 2023 AM62A3 , AM62A3-Q1 , AM62A7 , AM62A7-Q1 , AM68A , AM69A
After all the above changes, verify the new sensor name is listed in the properties of GStreamer plugin tiovxisp. For example, IMX219 is shown as below:
root@am62axx-evm:~# gst-inspect-1.0 tiovxisp
...
sensor-name : TIOVX camera sensor string ID. Below are the supported sensors
SENSOR_SONY_IMX219_RPI